S12X CAN Identifier Acceptance Filter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12X CAN Identifier Acceptance Filter

1,212 Views
shuchunliu
Contributor I

Hello,

For S12X, what is the difference between First Bank(CANIDAR0-7) and Second Bank(CANIDAR4–CANIDAR7)?

Labels (1)
0 Kudos
Reply
1 Reply

1,069 Views
RadekS
NXP Employee
NXP Employee

Hi Shuchun,

There isn’t any significant difference between first and second filter bank except rule in identifier hit flags (CANIDAC_IDHIT[2:0]) – If more than one hit occurs (two or more filters match), the lower hit has priority.

The Identifier Acceptance Filters are independent.

BTW: I suppose that you mean First Bank(CANIDAR0-3)

The Identifier Acceptance Filters could be configured to:

1.    Two 32bit filter banks,

2.    or four 16bit filter banks,

3.    or eight 8bit filters.

Tested are the full identifiers or the most significant bits from identifier (and RTR, IDE, SRR bits) when identifier is longer than filter.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply