S12G192, can transmit, after set CANXTFLG = CANXTBSEL, busoff, synch lost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12G192, can transmit, after set CANXTFLG = CANXTBSEL, busoff, synch lost

725件の閲覧回数
xiujuantang
Contributor II


Hi,

 

I have no idea how I can get busoff state after CANXTFLG = CANXTBSEL to set TXE as full.

 

Br

Cindy

ラベル(1)
0 件の賞賛
返信
1 返信

650件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Cindy,

The MSCAN module will go into busoff state when TX error counter reach value 255. Several types of error could increase TX error counter, but the simplest way how to get busoff state is transmitting any CAN message while we short CANH and CANL lines.

I hope it helps you.


Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信