S12G Flash Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12G Flash Driver

1,462件の閲覧回数
secrob
Fresh Out Contributor

I would really appreciate if someone knows about S12G Driver Flash spec: at first I'm unable to understand if the built-in algorithms, accessible on Flash memory via pre-defined register, run on RAM or are somewhere written in rom...Then is there their availability as done for PPC (C90FL driver executables for example) anywhere in the Freescale material? Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,328件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

I recommend you to analyze the Application Note AN3275, it has a detailed explanation on the eeprom functionality and it also has a software sample in which you can refer to source file s12eeprom.c to view the eeprom routines. I have attached the AppNote to this response.