S12G Flash Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12G Flash Driver

1,411 Views
secrob
Contributor II

I would really appreciate if someone knows about S12G Driver Flash spec: at first I'm unable to understand if the built-in algorithms, accessible on Flash memory via pre-defined register, run on RAM or are somewhere written in rom...Then is there their availability as done for PPC (C90FL driver executables for example) anywhere in the Freescale material? Thanks

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,277 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

I recommend you to analyze the Application Note AN3275, it has a detailed explanation on the eeprom functionality and it also has a software sample in which you can refer to source file s12eeprom.c to view the eeprom routines. I have attached the AppNote to this response.