S12 project's Compiler Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12 project's Compiler Error

3,033件の閲覧回数
菜緒西井
Contributor III

Hello.

I use CW v10.7 and MC9S12ZVML128 PMSM Sensorless.

I used "not latest" projects ,so I installed latest package (AN5327_SW_CW10 and MTRCKTSPNZVM128_CW10).

And I installed MC9S12ZVM_AMMCLIB_v1.1.11.

Then, I tried to build these, but I got errors (Compiler Error).

I reinstalled CW and SW, AMMCLIB, but errors don't disappear.

I can build "not latest" projects, but the latest projects can't.

Isn't there something error in the latest file?

Or my installed files are something wrong?

If you know the cause or solution, please let me know.

For detail of the error, please check an attached file.

The error is very long, so file's error is part of all log.

(The error of AN5327 and MTRCKTSPNZVM128 are almost same.)

Best regards,

Nao

2 返答(返信)

2,870件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Nao,

I tried it and I can compile the project without any errors in the CW 10.7 and I also tried CW 11.0 - there can be some updates which fix this errors.

Could you try install CW v11.0: CodeWarrior for Microcontrollers-Eclipse IDE|NXP ?

Let me know, how it works.

Best regards,

Diana

2,870件の閲覧回数
菜緒西井
Contributor III

Hello, Diana Batrlova.

Thank you for your advice.

I tried CW v11.0, but it works same as v10.7.

Also, I can build "not latest" projects at v11.0.

For detail of the error, please check images.

build_error_v11.PNG

build_error2_v11.PNG

Please let me know if you know the cause of these errors.

Best regards,

Nao.

0 件の賞賛
返信