S12 Bootloader example for Cosmic Compiler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12 Bootloader example for Cosmic Compiler

2,753件の閲覧回数
Gildarai
Contributor II

Hello all.

I'm looking for bootloader example for cosmic compiler.

I've found example "AN5389SW", but it looks like just for a Code warrior.

I tried convert that example, but there are some difference from grammar such like below.

#pragma CODE_SEG DEFAULT_RAM

void PFLASH_Send_Command(void)

{

asm PSH CCL; // 0x10 command

DisableInterrupts;

 

FSTAT_CCIF = 1; //launch command

while(FSTAT_CCIF == 0){}; //wait for done

 

asm PUL CCL; // 0x90 command

}

 

Do you have documents or example for what help to me make a bootloader for Cosmic compiler?

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,750件の閲覧回数
Gildarai
Contributor II

Additionally, 

 

Is it possible to apply and work that Bootloader made by CW, Application made by Cosmic?

I have both Code warrior and Cosmic compiler, so if possible that, I can try it.

0 件の賞賛
返信

2,687件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Gildarai,

You can definitely try to adjust the code using vendor specfic options.

I'd recommend you to check the attached Technical note for more details about differences between CodeWarrior and Cosmic:

 

Hope it helps.

Stan

 

 

0 件の賞賛
返信