Hello,
There is any possible way to detect a connected BDMPod to the controller in a runing firmware ?
My target is realtime bypassing of the wai and stop instructions while debugger are connected.
I very rarely using the debugger and I always stuck on same problem.
Because my firmware uses wai and stop the debugger can't connect and/or freezes when thh processor going to sleep.
so I always spend of hours to finding the problem, why de debugger is freezes....
I know I'm stupid a little...
My another question is, any easy way to disable all interrupts when I stopped and using trace command ?
currently im mods the CCR by hand to disable the interrupts.
I'm using BDMPod with Firmware: 6.0.0b17, Bootloader Version: 2.0.6 with S12G, S12VR, S12XS processors.
已解决! 转到解答。
Hi Ferenc,
Unfortunately, my experiences with LFBDMPGMR are quite limited.
 
I am afraid that BDM connection is not the right tool for debugging MCU which going into stop mode.
The clocks are disabled and BDM connection lost in that case.
I think that you probably need some tool for real-time debugging. I would like to recommend for example Freemaster:
http://www.nxp.com/products/power-management/wireless-charging-ics/freemaster-run-time-debugging-too...
You may read/modify/write variables/register/… during run-time. It typically uses some serial channel like SCI for communication.
The disadvantage is that you need to implement and service serial driver in your code.
Note: The CPU can not enter a low power mode (stop or wait) during BDM active mode.
Yes, you may set I bit for mask all I-bit maskable interrupts.
Currently, I do not have any other idea how to do a different way.
Note: If your application uses COP, I would like to recommend trying to set RSBCK bit for stop the COP and RTI in Active BDM mode.
I hope it helps you.
Have a great day,
Radek
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ferenc,
Since most of BDM debuggers most of the time start the debug session from resetting target into special single chip mode, you may detect it like this
// wasn't BKGD pulled low at poweron / reset?
      if(MODE & MODE_MODC_MASK)
      {
             // no, it was high and not pulled low by BDM dongle
// ,normal operating mode, we can WAI...
              asm("WAI");
       }
Hi Ferenc,
Unfortunately, my experiences with LFBDMPGMR are quite limited.
 
I am afraid that BDM connection is not the right tool for debugging MCU which going into stop mode.
The clocks are disabled and BDM connection lost in that case.
I think that you probably need some tool for real-time debugging. I would like to recommend for example Freemaster:
http://www.nxp.com/products/power-management/wireless-charging-ics/freemaster-run-time-debugging-too...
You may read/modify/write variables/register/… during run-time. It typically uses some serial channel like SCI for communication.
The disadvantage is that you need to implement and service serial driver in your code.
Note: The CPU can not enter a low power mode (stop or wait) during BDM active mode.
Yes, you may set I bit for mask all I-bit maskable interrupts.
Currently, I do not have any other idea how to do a different way.
Note: If your application uses COP, I would like to recommend trying to set RSBCK bit for stop the COP and RTI in Active BDM mode.
I hope it helps you.
Have a great day,
Radek
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------