Register range can edit or not

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Register range can edit or not

ソリューションへジャンプ
1,718件の閲覧回数
Neo_zhang
Contributor II

MC9S12DT256CPVE  0x0-0x3ff range is register, can it be written to all FF? Does this matter when I copy One chip  to  another?

タグ(1)
0 件の賞賛
返信
1 解決策
1,694件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

The registers are RAM memory which loses content after power off. Each reset sets the registers to reset values described for each register in the data sheet. Some of the register are write once only which means that after the first write they are not re-writable till next reset. Also there are register which are loaded during reset automatically by a value stored in special fields of the flash memoroy (like register FPROT, FSEC, COPCTL,…)

When you copy content of one MCU to another the content of the register has no meaning because, as I wrote above, the content is either defined after reset (reset value of the register) or loaded from the special field (setup registers for security, protection, COP, ….)

 

Best regards,

Ladislav

元の投稿で解決策を見る

1 返信
1,695件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

The registers are RAM memory which loses content after power off. Each reset sets the registers to reset values described for each register in the data sheet. Some of the register are write once only which means that after the first write they are not re-writable till next reset. Also there are register which are loaded during reset automatically by a value stored in special fields of the flash memoroy (like register FPROT, FSEC, COPCTL,…)

When you copy content of one MCU to another the content of the register has no meaning because, as I wrote above, the content is either defined after reset (reset value of the register) or loaded from the special field (setup registers for security, protection, COP, ….)

 

Best regards,

Ladislav

%3CLINGO-SUB%20id%3D%22lingo-sub-1848036%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E7%AF%84%E5%9B%B2%E3%81%AF%E7%B7%A8%E9%9B%86%E5%8F%AF%E8%83%BD%E3%81%8B%E3%81%A9%E3%81%86%E3%81%8B%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1848036%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EMC9S12DT256CPVE%200x0-0x3ff%E3%81%AE%E7%AF%84%E5%9B%B2%E3%81%AF%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%81%A7%E3%81%99%E3%81%8C%E3%80%81%E3%81%99%E3%81%B9%E3%81%A6%E3%81%AEFF%E3%81%AB%E6%9B%B8%E3%81%8D%E8%BE%BC%E3%82%80%E3%81%93%E3%81%A8%E3%81%8C%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%81%8B%3F%E3%81%93%E3%82%8C%E3%81%AF%E3%80%81%E3%81%82%E3%82%8B%E3%83%81%E3%83%83%E3%83%97%E3%82%92%E5%88%A5%E3%81%AE%E3%83%81%E3%83%83%E3%83%97%E3%81%AB%E3%82%B3%E3%83%94%E3%83%BC%E3%81%99%E3%82%8B%E3%81%A8%E3%81%8D%E3%81%AB%E5%95%8F%E9%A1%8C%E3%81%AB%E3%81%AA%E3%82%8A%E3%81%BE%E3%81%99%E3%81%8B%3F%3C%2FP%3E%3C%2FLINGO-BODY%3E