Regarding number of timer zero channels available for 48 pin ZVM16 MCU.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding number of timer zero channels available for 48 pin ZVM16 MCU.

899 次查看
pratibhasurabhi
Contributor V

Hi,

I want to know the number of timer zero channels in ZVM16(48 pin) MCU.

In Pin out diagram of ZVM16(48 pin) MCU only one channel is shown as below in yellow mark,

pastedImage_3.png

I want to confirm, is there only one channel of timer zero or other channels are there?

Its urgent,please inform me the answer of same as early as possible.

Thanks.

0 项奖励
回复
2 回复数

758 次查看
RadekS
NXP Employee
NXP Employee

Hi Pratibha,

It seems that you probably have some older version of reference manual.

The current version 2.11 shows also routing option for IOC0_1 and IOC0_2 at pins PS0 and PS1.

S12ZVMpinoutLQFP48.png

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

758 次查看
pratibhasurabhi
Contributor V

Thank you Radek for quick reply!

0 项奖励
回复