Regarding Cosmic Compiler for Freescale S12G128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding Cosmic Compiler for Freescale S12G128

2,269 Views
arjunreddy
Contributor I

Hello Everyone,

 

For preprocessing iam using gcc, for compiling and linking iam using Cosmic compiler. But after preprocessing, during compilation phase it showing error as"bad # syntax". This is because while preprocessing gcc will add # and line to includes. But this syntax is not accepting in cosmic compiler. Any compiler option or flag is available to suppress this error?

 

 

Another thing is cxs12x.exe(compiler for cosmic) is doing process from parser to code generater to compilation. Is any option to use cxs12x only as compiler?

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,635 Views
lama
NXP TechSupport
NXP TechSupport

Have yu tried to contact cosmic help line Cosmic Software - Support

(Cosmic Software - Contact Information)

best regards,

Ladislav

0 Kudos
Reply

1,635 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g.CodeWarrior Development Tools or 16-bit Microcontrollers )  to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 Kudos
Reply