Reg. Erase / Write Cycles for EEPROM - MC9S12DJ64

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reg. Erase / Write Cycles for EEPROM - MC9S12DJ64

2,332 次查看
balajiprabhakar
Contributor I
Hi All,
 
In MC9S12DJ64 controller, How many ERASE/WRITE cycles are guaranteed for the EEPROM.
 
with regards,
 
Ganansekar.
标签 (1)
0 项奖励
回复
2 回复数

1,085 次查看
Lundin
Senior Contributor IV
The manual (A.32 NVM Reliability) says min 10000 cycles in temperatures below 0 dgr C, and min 100000 cycles in temperatures above 0 dgr C.
0 项奖励
回复

1,085 次查看
e_taylor
Contributor III
hello:
 
i don't know the value off hand but it should be listed under electrical spefications. the spec is for the entire temperature range and unless you are using the board in harsh temperatures the number is actually quite a low estimate.
 
 
regards,
 
ed
0 项奖励
回复