Question on TJA1043

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,174件の閲覧回数
nadeem_syed
Contributor I

In our application, pins VBAT (pin 10) and WAKE (pin 9) are tied together. Our application matches with the information shown in Section.12 Example Application diagram of datasheet.

I have following question

1. When we provide VBATT (12V) to our application we are observing "INH" signal turns on.
I believe TJA1043 device considers this as a local wake-up event and turns on "INH" signal. Is my understanding correct ?

2. What will be the operating mode of TJA1043 device when VBATT is turned off ?

0 件の賞賛
返信
1 解決策
3,139件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

transceiver's behavior after Vbat connection is described in chapter "Software flow for an ECU cold start" of AH1014 (page 67).

 

BR, Petr 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,169件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

1) when Vbat is applied, transceiver goes to Standby mode, INH pin is pulled up to Vbat. Once EN and STBN pins becomes driven by the MCU, a mode is determined by their level, for example if driven high transceiver enters Normal mode.

2) if there is undervoltage only on Vbat then device is in Standby mode. If there is undervoltage on Vio or Vcc then device go to Sleep mode.

 

See more in AH1014; https://www.nxp.com/documents/report/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pdf

 

BR, Petr

 

0 件の賞賛
返信
3,161件の閲覧回数
nadeem_syed
Contributor I

Can you please explain a little bit more detail about why the device pulls INH pin up to VBAT when the VBAT is applied ?

Is this because the pins VBatt & Wake are tied together ? Is the device considering this as a local wake-up event ?

0 件の賞賛
返信
3,140件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

transceiver's behavior after Vbat connection is described in chapter "Software flow for an ECU cold start" of AH1014 (page 67).

 

BR, Petr 

0 件の賞賛
返信