Question for stall error GDUDSE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question for stall error GDUDSE

1,271 Views
minggangnie
Contributor I

Hi,

 .

I'm using S12ZVML128 on my own PCB.

Motor is 240W,  12V, 20A

Motor can alignmen,But can't open loop start.

hardware parameter :  I MAX 40A                U DCB MAX 25V

Register GDUDSE=0X70

0 Kudos
Reply
1 Reply

1,150 Views
RadekS
NXP Employee
NXP Employee

Hi Minggang,
Desaturation error:
If the high-side power FET is turned on and the drain source voltage VDS is greater than Vdesaths after the blanking time tBLANK a desaturation error will be flagged. In this case, the associated desaturation error flag GDHSIF[2:0] will be set and the high-side power FET will be turned off. The level of the voltage Vdesaths can be adjusted in the range of 0.35 to 1.40V in GDUDSLVL register.

I suppose, that issue will be probably in some incorrect settings or hardware connection.
Could you share with us your schematic for short review?

I suppose, that you use one of reference projects as a template.
http://www.nxp.com/products/software-and-tools/run-time-software/automotive-software-and-tools/motor...
Could you please share with us your project or at least your settings for short review?

If any of this information are not public, you may create service ticket:
https://community.nxp.com/docs/DOC-329745

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply