Question about initialization in 3-phase Sensorless BLDC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about initialization in 3-phase Sensorless BLDC

1,284 Views
菜緒西井
Contributor III

Hello Team,

I use MC9S12ZVML128_BLDC_Sensorless example project.

Why set the duty to 50% at initialization?

0 Kudos
Reply
1 Reply

1,138 Views
pachamatej
NXP Employee
NXP Employee

Hello, could you please check out the new software package on the web? 3-phase Sensorless BLDC Development Kit|NXP  I believe the 50% duty-cycle initial setting is not presented there.

However, if the switching strategy is a bi-polar switching, then it would be a good idea to set a neutral duty-cycle at the very start.

BR

Matej

0 Kudos
Reply