Programming S9S12G64F0CLF sanity check

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming S9S12G64F0CLF sanity check

Jump to solution
1,635 Views
robert_anderson
Contributor I

I'm attempting to program the S9S12G64F0CLF microcontroller using the PEMicro Cyclone. To do that, I want to create a single .sap file with the calibration, bootloader, and application files all in one. In the image creation tool, I have the software set as such:

 

CPU Manufacturer: NXP

Target Architecture: HC9(S)12(X)

Programming Sequence:

CM Freescale_9S12G64_1x16x32k_64k_Linear_Pflash.12P

EM

QO BOOTLOADER

PM

VM

CQ

QO APPLICATION

PM

VM

CQ

CM Freescale_9S12G64_1x16x1k_2k_EEPROM.12P

QO CALIBRATION

PM

VM

Ignore Address Range Check box checked.

 

Does this look like the correct way to create the .sap file?

 

Thank you.

0 Kudos
Reply
1 Solution
1,615 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

 

this is the 3rd part product. You should contact www.pemicro.com support in this case.

 

Best regards,

Ladislav

View solution in original post

0 Kudos
Reply
1 Reply
1,616 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

 

this is the 3rd part product. You should contact www.pemicro.com support in this case.

 

Best regards,

Ladislav

0 Kudos
Reply