Programming S9S12G64F0CLF sanity check

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming S9S12G64F0CLF sanity check

ソリューションへジャンプ
1,630件の閲覧回数
robert_anderson
Contributor I

I'm attempting to program the S9S12G64F0CLF microcontroller using the PEMicro Cyclone. To do that, I want to create a single .sap file with the calibration, bootloader, and application files all in one. In the image creation tool, I have the software set as such:

 

CPU Manufacturer: NXP

Target Architecture: HC9(S)12(X)

Programming Sequence:

CM Freescale_9S12G64_1x16x32k_64k_Linear_Pflash.12P

EM

QO BOOTLOADER

PM

VM

CQ

QO APPLICATION

PM

VM

CQ

CM Freescale_9S12G64_1x16x1k_2k_EEPROM.12P

QO CALIBRATION

PM

VM

Ignore Address Range Check box checked.

 

Does this look like the correct way to create the .sap file?

 

Thank you.

0 件の賞賛
返信
1 解決策
1,610件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

 

this is the 3rd part product. You should contact www.pemicro.com support in this case.

 

Best regards,

Ladislav

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,611件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

 

this is the 3rd part product. You should contact www.pemicro.com support in this case.

 

Best regards,

Ladislav

0 件の賞賛
返信