Programmer for S12Z microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programmer for S12Z microcontroller

2,816 Views
fadi-eid
Contributor II

Dear NXP Community, I am looking for a BDM programmer to program the S912ZVML12F3WKH microcontroller. I found this one on Amazon.com for a reasonable price. The seller says in the description that it supports the HCS12.

fadieid_0-1710423108883.pngfadieid_0-1710423108883.png

 

After some search, I wasn't able to find if this programmer can program the S12Z MCU (S912ZVML12F3WKH). What made it more confusing is that MC9S12ZVM-Family
Reference Manual, in the first page, mentions "HCS12 microcontrollers".

fadieid_1-1710423149182.pngfadieid_1-1710423149182.png

 

 

Tags (3)
0 Kudos
Reply
3 Replies

2,783 Views
lama
NXP TechSupport
NXP TechSupport

There are basically 2 ways how to program S12Z in CodeWarrior(Eclipse):
1) via Debug Configuration (Assume you are using Pemicro debug probe)
2) via Flash programmer (Target Task configuration)

Another way is programmer which is provided by www.pemicro.com or another company.


If you use option #1 I'd suggest to consider program the device using Target Task. Simply create a new target task, configure the flash memory and programming sequence.

lama_0-1710758267553.pnglama_0-1710758267553.png

 




lama_1-1710758267590.pnglama_1-1710758267590.png

 

lama_2-1710758267611.pnglama_2-1710758267611.png

 





You can also execute Target Task scripts from the debugger console.
Hope it helps.

0 Kudos
Reply

2,772 Views
fadi-eid
Contributor II

Thank you for your reply. So if I understood well, there is no need to buy a programming software, I can program the S12Z using PE Micro Universal Multilink programmer and use Code Warrior for free.

0 Kudos
Reply

2,754 Views
stanish
NXP Employee
NXP Employee

As far as I know, you don't need any extra programming software. You can use free version (called special edition) of CodeWarrior for MCUs 11.x  integrated flash programmer tool to program your S12Z MCU using Pemicro probe.

Hope it helps.

Stan

0 Kudos
Reply