Programmer for S12Z microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programmer for S12Z microcontroller

2,890件の閲覧回数
fadi-eid
Contributor II

Dear NXP Community, I am looking for a BDM programmer to program the S912ZVML12F3WKH microcontroller. I found this one on Amazon.com for a reasonable price. The seller says in the description that it supports the HCS12.

fadieid_0-1710423108883.png

 

After some search, I wasn't able to find if this programmer can program the S12Z MCU (S912ZVML12F3WKH). What made it more confusing is that MC9S12ZVM-Family
Reference Manual, in the first page, mentions "HCS12 microcontrollers".

fadieid_1-1710423149182.png

 

 

タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,857件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

There are basically 2 ways how to program S12Z in CodeWarrior(Eclipse):
1) via Debug Configuration (Assume you are using Pemicro debug probe)
2) via Flash programmer (Target Task configuration)

Another way is programmer which is provided by www.pemicro.com or another company.


If you use option #1 I'd suggest to consider program the device using Target Task. Simply create a new target task, configure the flash memory and programming sequence.

lama_0-1710758267553.png

 




lama_1-1710758267590.png

 

lama_2-1710758267611.png

 





You can also execute Target Task scripts from the debugger console.
Hope it helps.

0 件の賞賛
返信

2,846件の閲覧回数
fadi-eid
Contributor II

Thank you for your reply. So if I understood well, there is no need to buy a programming software, I can program the S12Z using PE Micro Universal Multilink programmer and use Code Warrior for free.

0 件の賞賛
返信

2,828件の閲覧回数
stanish
NXP Employee
NXP Employee

As far as I know, you don't need any extra programming software. You can use free version (called special edition) of CodeWarrior for MCUs 11.x  integrated flash programmer tool to program your S12Z MCU using Pemicro probe.

Hope it helps.

Stan

0 件の賞賛
返信