Programm EEPROM MC9S12XDP512 without BDM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Programm EEPROM MC9S12XDP512 without BDM

跳至解决方案
2,554 次查看
admin
Specialist II
Hello.
In my program it is necessary to save current customisations in EEPROM. I work with microprocessor MC9S12XDP512. Has written the program I start it in a debug mode with connected BDM modul, all perfectly works. I disable BDM modul I include the device, it passes in a state an error of operation with EEPROM. I can not understand why so occurs (((((. I think that probably occurs from for that that a normal operating mode of the microprocessor the writeprotect is installed. Read datasheet there it is written that it can be removed with the help backdoor key access, but I have not found what data series it would be necessary to write what to remove protection ((((   Prompt as to be????
标签 (1)
0 项奖励
回复
1 解答
1,398 次查看
kef
Specialist I

If I understood you properly, EEPROM works in special mode (with BDM connected), and doesn't work in normal mode. ECLKDIV register is write-once in normal modes. Make sure your code initializes ECLKDIV using single write operation. For example setting/clearing PRDIV8 bit, then writing other ECLKDIV bits is bad and won't work in normal modes.

 

Backdoor access has nothing to do with write protection.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,399 次查看
kef
Specialist I

If I understood you properly, EEPROM works in special mode (with BDM connected), and doesn't work in normal mode. ECLKDIV register is write-once in normal modes. Make sure your code initializes ECLKDIV using single write operation. For example setting/clearing PRDIV8 bit, then writing other ECLKDIV bits is bad and won't work in normal modes.

 

Backdoor access has nothing to do with write protection.

0 项奖励
回复
1,398 次查看
admin
Specialist II
Thanks kef, in it also there was a problem))))
0 项奖励
回复