Processor Expert for MC68HC912D60A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert for MC68HC912D60A

1,997件の閲覧回数
Karla
Contributor I
Hello,

I am a student at the University of Texas at El Paso and I am using the MC68HC912D60A for a project. As part of the project, I am implementing an FFT. I recently found an FFT bean for the HCS12 in the Processor Expert website, so I was wondering if this bean could be used with the MCU I am using, or if there is a similar bean for the
MC68HC912D60A. Moreover, when creating a new project in Code Warrior and selcting the MC68HC912D60A, the option to use Processor Expert is not available. Is there a version of this software to be used with the MC68HC912D60A?

Regards,


ラベル(1)
1 返信

1,148件の閲覧回数
CrasyCat
Specialist III
Hello
 
ProcessorExpert is available only for HCS12 and HCS12X CPUs.
Legacy HC12 CPUs are not supported by ProcessorExpert.
 
CrasyCat