Problems with TWR-S12G128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with TWR-S12G128

1,228件の閲覧回数
laurenfulton
Contributor I

I am having an intermittent problem with a TWR-S12G128 board.  Sometimes it works fine.  With nothing changing, Code Warrior suddenly cannot communicated with it. If I try to unplug the USB and reattach it, I frequently get an error message of “USB Device Not Recognized, One of the USB devices attached to this computer has malfunctioned, and Windows does not recognize it.” I have had this problem on multiple computers. Help?

ラベル(1)
0 件の賞賛
返信
1 返信

1,100件の閲覧回数
Martin35804
NXP Employee
NXP Employee

If you are using the OSBDM please try to change the USB cable and if this doesn't help then the section of the board that is responsible for the OSBDM programming is experiencing a failure.

In such cases we recommend to use PEmicro programmer either the USB Multilink or Universal Multilink  connected to proper BDM headers on the board.

I hope this will help.

0 件の賞賛
返信