Problems implementing CAN on MC9S12XEP100 DEMO Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems implementing CAN on MC9S12XEP100 DEMO Board

2,024件の閲覧回数
ace386
Contributor I

Hi,

we tried to implement MSCAN on mentioned Board and encountered following problem:

The example code from the archive found under "rdhcs12caniomodsw" won't compile complaining about incompatible memory models "small" and "banked". Changing from "banekd" to "small" in the project settings in CodeWarrior won't solve the problem but lead to even more errors of the same type.
Manually changing the header files leads to a compilable project - as long as no CAN-specific function is called during the program!

Also, using code from AN2726 won't compile because of multiple definitions in some header files (we inluded the project's headers plus the chip-specific header for MC9S12XEP100), that can't be resolved by commenting the affected lines.

Is there any known working (MS)CAN example for MC9S12XEP100? Or are there any hints for us on how to get a simple CAN communication working between two of the mentioned DEMO Boards?

Thank you very much,
ace386

ラベル(1)
0 件の賞賛
返信
1 返信

1,078件の閲覧回数
jsmcortina
Contributor III

I have CAN running on the DEMO board, but found that C406 and C407 need to be removed to allow transmission at 0.5Mbps

 

I didn't use the supplied sample code. My application is "Megasquirt" aftermarket engine management and I have adapted the existing MC9S12C64 code.  The only changes required were the frequency dividers.

 

The source code for this is publicly available but only use it "for inspiration" as it is copyright.

 

James

0 件の賞賛
返信