Problem with debug : step to step

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with debug : step to step

Jump to solution
2,375 Views
chris69
Contributor I

Hi,

 

I have a mc9s12dg256, when i run my program in debug and i want to do step to step (F10 for example) but all the times i do step to step i step into the OSTickISR !

SO i can't debug with step.

 

Can anyone, please, help me 

Labels (1)
0 Kudos
Reply
1 Solution
1,930 Views
CrasyCat
Specialist III

Hello

 

If you are using a P&E Multilink/CyclonePro cable for debugging, if you select entry Communication or Connect in the Multilink/CyclonePro menu you open the connection dialog.

 

Inside of the Special Setup or Debug option tab you should be able to  find a box "Disable maskable ISRs when stepping".

 

Check it and you should be able to avoid stepping inside of the interrupt functions.

 

CrasyCat

View solution in original post

0 Kudos
Reply
2 Replies
1,931 Views
CrasyCat
Specialist III

Hello

 

If you are using a P&E Multilink/CyclonePro cable for debugging, if you select entry Communication or Connect in the Multilink/CyclonePro menu you open the connection dialog.

 

Inside of the Special Setup or Debug option tab you should be able to  find a box "Disable maskable ISRs when stepping".

 

Check it and you should be able to avoid stepping inside of the interrupt functions.

 

CrasyCat

0 Kudos
Reply
1,930 Views
chris69
Contributor I

thank you :smileyhappy:

0 Kudos
Reply