Problem with debug : step to step

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with debug : step to step

ソリューションへジャンプ
2,374件の閲覧回数
chris69
Contributor I

Hi,

 

I have a mc9s12dg256, when i run my program in debug and i want to do step to step (F10 for example) but all the times i do step to step i step into the OSTickISR !

SO i can't debug with step.

 

Can anyone, please, help me 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,929件の閲覧回数
CrasyCat
Specialist III

Hello

 

If you are using a P&E Multilink/CyclonePro cable for debugging, if you select entry Communication or Connect in the Multilink/CyclonePro menu you open the connection dialog.

 

Inside of the Special Setup or Debug option tab you should be able to  find a box "Disable maskable ISRs when stepping".

 

Check it and you should be able to avoid stepping inside of the interrupt functions.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,930件の閲覧回数
CrasyCat
Specialist III

Hello

 

If you are using a P&E Multilink/CyclonePro cable for debugging, if you select entry Communication or Connect in the Multilink/CyclonePro menu you open the connection dialog.

 

Inside of the Special Setup or Debug option tab you should be able to  find a box "Disable maskable ISRs when stepping".

 

Check it and you should be able to avoid stepping inside of the interrupt functions.

 

CrasyCat

0 件の賞賛
返信
1,929件の閲覧回数
chris69
Contributor I

thank you :smileyhappy:

0 件の賞賛
返信