Problem in linker file of Comic compiler for the .data and .bss sections

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in linker file of Comic compiler for the .data and .bss sections

1,244件の閲覧回数
ahmedfouda
Contributor I

I'm using cosmic compiler. For S12x micro controller.

 

In the linker file if I set the following

 

+seg .data       -b 0x2110 -o 0x2110 -m 0x1EF0  -n .data
+seg .bss                                       -n .bss

 

The System works fine but If I change it to

 

+seg .data       -b 0xFE000-o 0x2110 -m 0x1EF0  -n .data
+seg .bss                                       -n .bss

 

The system doesn't work.

 

The only difference is that in the second case I put the global address, Do you have any idea what is the problem.

I need to use the second option due to some constraints within my application.

ラベル(1)
0 件の賞賛
返信
1 返信

935件の閲覧回数
Pedro_
Contributor III

It would be best if you could provide info on how other segmets are configured.

For example, where is your stack? Why did you define your data with maximum size of 0x1EF0?

 

I believe the problem is that the physical and logical addresses don't match.

 

Try this:

+seg .data       -b 0xFE000 -o 0x2000 -m 0x1EF0  -n .data
+seg .bss        -a.data -n .bss

0 件の賞賛
返信