Problem for emulated EEPROM on S12XE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem for emulated EEPROM on S12XE

2,604 Views
zuqingzhu
Contributor I

Recentally we receive some failed modules, according to the failure reports, the failure are always happened when the module is powered up.

According to the test result, we find the program is always stuck in below while(1), that means the failed modules will be reset again and again. Does it mean that program to clear error flag of FSTAT and FERFSTAT should be added before module reset?

This module had been released to market for several years, but the failed modules are only found in the modules manufactured in last year. Why? Does it mean that CPU reset could clear these error flags for old S12XE chips, but not for the new chips manufactered in last year? Please advise. Thank you.

status=LaunchFlashCommand(0 ,ENABLE_EEPROM_EMULATION, 0, 0, 0, 0, 0, 0);
  if(((status.fstat_var&0x33)!=0)||((status.ferfstat_var&0xDF)!=0))
   {
    normal_rst1=0xAA;
    normal_rst2=0xAA;
    while(1);
   }

0 Kudos
Reply
6 Replies

2,396 Views
kef2
Senior Contributor V

Jason,

It's a pity you don't know which FSTAT or FERSTAT bits led to the problem.

Do you provide any real means to prevent power loss during EEE write to flash operation? If not I would expect some errors sometimes due to incomplete write/erase on power down. The question is are such errors recoverable without repartition or not. 

I would try issuing EEE query command to check whether xxPART parameters are OK and to know how big is erase count.

0 Kudos
Reply

2,396 Views
zuqingzhu
Contributor I

Hi Edward,

Thank you for the suggestion. I'll try to issue EEE query command to request EEE status. But up to now, we can't reproduce the failure in our test lab. Is it possible EMC issue on site resulted in the errors of FSTAT and FERSTAT registers?

Best Regards,

Jason Zhu

0 Kudos
Reply

2,396 Views
kef2
Senior Contributor V

Hi Jason,

  •  Is it possible EMC issue on site resulted in the errors of FSTAT and FERSTAT registers?

I doubt it, more likely EMC caused reset during write/erase.

Best Regards,

Edward

0 Kudos
Reply

2,396 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

I would like to suggest you to compare your approach to example which is working - see atachment.

There is no info how you process the EEEPROM in your example.

Some more examples you can find at:

LAMA's S12XE unofficial examples 

Best regards,

Ladislav

0 Kudos
Reply

2,396 Views
zuqingzhu
Contributor I

Hi Iama,

Thank you for the example.

According to AN3743, if errors of FSTAT and FERSTAT registers are detected, the user should use software to mitigate the occurrence and clear the error flag. But I can't find out example code in AN3743SW example or your attached example. Any example code for my reference?

Best Regards,

Jason Zhu

0 Kudos
Reply

2,396 Views
lama
NXP TechSupport
NXP TechSupport
0 Kudos
Reply