Problem connecting to HCS12X board using a Processor Expert project through serial monitor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem connecting to HCS12X board using a Processor Expert project through serial monitor

1,684件の閲覧回数
Mounties
Contributor I

We are encountering errors when debugging.  We're only using the asynchronous bean, AS1-AnsynchroSerial.  The error generated is "CommError: 00000008 =  CE_FRAME; InQue: 5, OutQue: 0".  Any ideas as to what may be causing this or typical scenarios that generate this error?

ラベル(1)
0 件の賞賛
返信
1 返信

1,299件の閲覧回数
Mounties
Contributor I

We are pretty sure that the problem are based on the CPU settings and we're wondering if anyone knows the correct CPU settings for ProcessorExpert to work?

0 件の賞賛
返信