Problem about BLDC hallEdgePeriod

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem about BLDC hallEdgePeriod

1,054 次查看
sufree
Contributor II

Hi,

   I use the AN4718SW to control BLDC motor with Hall sensor,and I have some problems about hallEdgePeriod which are  used to caculate actual speed as the following way:

period6ZC = hallEdgePeriod[1] + hallEdgePeriod[2] + hallEdgePeriod[3] + \
hallEdgePeriod[4] + hallEdgePeriod[5] + hallEdgePeriod[6];

actualSpeed = SPEED_CALC_NUMERATOR / period6ZC;

I have two problems:

  • 1、When the speed  in 500,1000,2000,2500RPM the hallEdgePeriod is correct,but when speed exceed 2500 ,for example 3000RPM ,there some wrong about  hallEdgePeriod as the following picture show,the hallEdgePeriod[2] and hallEdgePeriod[4]'s value suddenly become smaller,the hall sensor  works normally.

  • 2、Why hallEdgePeriod 1,3,5 and hallEdgePeriod 2,4,6 have similar value that are vary widely. Shouldn't it be the same?

vds.PNG

0 项奖励
回复
0 回复数