Problem Program Module MC9S12XDP512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem Program Module MC9S12XDP512

1,972件の閲覧回数
MicroHit
Contributor I
Hi, I 've Cyclon Pro to Program a  Microcontroler MC9S12XDP512 .
When select the module software algorithm Freescale_MC9S12XDP512_1X16_2k_4k_EEPROM_linear_4k_page.12P
the Base Adress=13F000.
Then try to Program Module and the message error is :
Invalid Addresses in srecord block from $0000C000 to $0000C01F.
 
 
What I am do Wrong ?
 
 
ラベル(1)
0 件の賞賛
返信
1 返信

1,212件の閲覧回数
Lundin
Senior Contributor IV
I assume that you are using PROG12Z? That's what it looks like anyway...

P&E have two different algorithms for every derivate: one for the banked flash and one for the eeprom. When programming the flash, you need to use a .phy file, which the contains "physical addresses" of the memory. In plain english this means that the P&E equipment can't handle common s-records when you are using addresses larger than 16-bit. This is not a problem however, since Codewarrior generates a .phy file, which ends up in the \bin directory of your project. Use that file for the flash.

When the flash programming is done, pick the algorithm for the eeprom instead. You'll be asked to enter the memory offset where your eeprom starts. If PROG12Z complains about some addresses that are out of range, let it ignore and continue.
0 件の賞賛
返信