Power supply components optimization for S12ZVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power supply components optimization for S12ZVM

ソリューションへジャンプ
1,835件の閲覧回数
ankur_kala
NXP Employee
NXP Employee

Hi,

 

The customer does not require Boost section as the power supply is regulated and would never go below 10V. Can the L, C, D associated with boost be completely avoided. Does he need to take care of anything else.

 

Also for the charge pump, customer saturates the duty cycle at 90% which means he would never be working on 100% duty cycle. Is it safe to say that the combination of C & D for charge pump section can be removed? Does he need to take care of these power pins of MCU in any special way.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,668件の閲覧回数
iggi
NXP Employee
NXP Employee

The Boost Converter is an option. So if customer would not use it, the external components are not necessary at all. The BST pin can be left floating, assuming the Boost option is disabled (by default bit GBOE = 0 in GDU Module Enable Register).

元の投稿で解決策を見る

2 返答(返信)
1,669件の閲覧回数
iggi
NXP Employee
NXP Employee

The Boost Converter is an option. So if customer would not use it, the external components are not necessary at all. The BST pin can be left floating, assuming the Boost option is disabled (by default bit GBOE = 0 in GDU Module Enable Register).

1,668件の閲覧回数
ankur_kala
NXP Employee
NXP Employee

Any idea if the charge pump needs to be there even if the duty in software is saturated?

0 件の賞賛
返信