Power supply components optimization for S12ZVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power supply components optimization for S12ZVM

Jump to solution
1,854 Views
ankur_kala
NXP Employee
NXP Employee

Hi,

 

The customer does not require Boost section as the power supply is regulated and would never go below 10V. Can the L, C, D associated with boost be completely avoided. Does he need to take care of anything else.

 

Also for the charge pump, customer saturates the duty cycle at 90% which means he would never be working on 100% duty cycle. Is it safe to say that the combination of C & D for charge pump section can be removed? Does he need to take care of these power pins of MCU in any special way.

Labels (1)
0 Kudos
Reply
1 Solution
1,687 Views
iggi
NXP Employee
NXP Employee

The Boost Converter is an option. So if customer would not use it, the external components are not necessary at all. The BST pin can be left floating, assuming the Boost option is disabled (by default bit GBOE = 0 in GDU Module Enable Register).

View solution in original post

2 Replies
1,688 Views
iggi
NXP Employee
NXP Employee

The Boost Converter is an option. So if customer would not use it, the external components are not necessary at all. The BST pin can be left floating, assuming the Boost option is disabled (by default bit GBOE = 0 in GDU Module Enable Register).

1,687 Views
ankur_kala
NXP Employee
NXP Employee

Any idea if the charge pump needs to be there even if the duty in software is saturated?

0 Kudos
Reply