Possibility to connect S12P64 to a display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Possibility to connect S12P64 to a display

835 Views
karimaremaka
Contributor I

Hello Team,

I would like to ask if it possible to program my µc Freescale S12P64 to be able to display some values and Strings in a desplay.

If it is possible, could you please provide me the source code, and the adequate Display that I can use (depending on the technology of transmission that you will provide me CAN/ TX-RX ...)

Please to be informed that I'm working with CodeWarrior Editor, and that I'm using the Freescale S12P64 µc.

Thanks in advance.

Tags (2)
0 Kudos
Reply
1 Reply

723 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

it is really up to yo which display you select from a market. The only limitation is a peripheral set of the MCU.

I have attached an example for S12G device. (you can directly use display routines for S12P). This code uses 2x16 display driven by HD44780 . If you want to use 4x20 display then you can look at differences in the setup ( file LCD_HD44780.H).

There is also description of functions  attached. I hope it will help you.

Best regards,

Ladislav

0 Kudos
Reply