Hello Nao Nishii,
The excel spreadsheet you refer to is an obsolete form of getting the parameters for control algorithm. This document is neither not supported nor shared any more. Please download and install the latest release of the SW package for given MCU platform.
https://www.nxp.com/downloads/en/evaluation-development-boards-systems/MTRCKTSPNZVM128_SW.exe
The latest SW package contains a FreeMASTER project with an MCAT tool. MCAT (Motor Control Application Tuning)tool is an NXP tool for tuning the control algorithm parameters.
Each control loop in the control structure behaves as a filter. To simplify the task, tuning the control loop means to tune the filter (cut-off frequency = bandwidth and attenuation).
Current loop - bandwidth in the range 100-300Hz, attenuation 0.7-1.
Speed loop - 10 times less than current loop bandwidth, attenuation = 1
Position observer bandwidth - up to 50Hz, attenuation 0.7-1.
For more details refer to the application note which is a part of installed package.
Regards,
Marek