Parallax RFID interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Parallax RFID interface

3,480 次查看
tcrite
Contributor II

Hi all,

 

This is my first post in the forums, so please forgive me in advance if it is not fully up to par. I'm trying to interface a parallax RFID reader to my MC9S12DG256 dragon board. The reader sends out 12 bytes of data with a start byte of 0x0A and a stop byte of 0x0D. I have the sout of the reader connected to pin PS2 of the dragon board. Here is the code I have written so far in Codewarrior:

 

#include <hidef.h>      /* common defines and macros */
#include <mc9s12dg256.h>     /* derivative information */

#pragma LINK_INFO DERIVATIVE "mc9s12dg256b"


char code[10];


void init_SCI1(void);
char getcSCI1(void);
void delay(int);
void init_PLL(void);
#define RDRF 1;

void main(){
  int val;
  int i;
  int bytesRead;
  init_SCI1();
 
  DDRJ |= 0x02;    // PJ1 outputs
  PTJ &= ~0x02;   // PJ1 = 0  to enable on-board LEDs for use with Port B
  DDRB = 0xFF;  // Port B outputs
 
  for(;:smileywink:{
    if((val = getcSCI1()) > 0){
      if(SCI1DRL == 0x0A){
        bytesRead = 0;
        while(bytesRead < 10){
          if(SCI1DRL > 0){
            val = getcSCI1();
            if((val == 0x0A) || (val == 0x0D)){
              break;
            }
            code[bytesRead] = val;
            bytesRead++;
          }
        }
      }
    }
    for(i = 10; i > 0; i--){
      PORTB = code[i];
      delay(1000);
    }
  }
}


/***************functions*****************/


void init_PLL( ){  // initializes phase-locked loop (hardware)for 24Mhz CPU clock
   asm(sei);        // for running board standalone w/out Codewarrior
   CLKSEL &= ~0x80;
   PLLCTL |= 0x40;
   SYNR = 0x05;
   REFDV = 0x01;
   while((CRGFLG & 0x08) == 0){ // wait here for lock
      CRGFLG |= 0x08;
   }
   CLKSEL |= 0x80;
   asm(cli);
}


void init_SCI1(){
  SCI1BDH = 0x02;  // Baud Div = 24MHz/(16x2400) = 625 =0x271
  SCI1BDL = 0x71;    // MSB of baud rate registers
  SCI1CR1 = 0x00;
  SCI1CR2 = 0x04;    // enable receive
}

char getcSCI1(){
  while(!(SCI1SR1 & 1)){}
  return (SCI1DRL);
}

void delay(int del){
  int i,j;
    for(i=0; i<del; i++)
       for(j=0; j<2000; j++);   
}

 

 

Any help would be greatly appreciated. Thanks.

标签 (1)
6 回复数

2,990 次查看
tcrite
Contributor II

Please disregard this post. I found what I was doing wrong.

2,990 次查看
hull
Contributor I

Glad, you get the bug out. I am also interested in interfacing the Parallax RFID to the Dragon board. Can you share your working code. Thanks.

2,990 次查看
tcrite
Contributor II

No problem. I'm sorry if it looks kinda sloppy, I haven't put in comments yet. I'm using Tera Term to output the tag id.

 

#include <hidef.h>      /* common defines and macros */
#include <mc9s12dg256.h>     /* derivative information */
#include "TERMIOSCI.H"
#include <stdio.h>

#pragma LINK_INFO DERIVATIVE "mc9s12dg256b"


char code[11];


void init_SCI1(void);
char getcSCI1(void);
void delay(int);
void init_PLL(void);
#define RDRF 0x20;

void main(){
  init_SCI1();
  init_PLL();
  TERMIO_Init();
 
  DDRJ |= 0x02;    // PJ1 outputs
  PTJ &= ~0x02;   // PJ1 = 0  to enable on-board LEDs for use with Port B
  DDRB = 0xFF;  // Port B outputs
  SCI0BDL = 156;
 
  for(;:smileywink:{}
    
}


/***************functions*****************/


void init_PLL(){  // initializes phase-locked loop (hardware)for 24Mhz CPU clock
   asm(sei);        // for running board standalone w/out Codewarrior
   CLKSEL &= ~0x80;
   PLLCTL |= 0x40;
   SYNR = 0x05;
   REFDV = 0x01;
   while((CRGFLG & 0x08) == 0){ // wait here for lock
      CRGFLG |= 0x08;
   }
   CLKSEL |= 0x80;
   asm(cli);
}


void init_SCI1(){
  SCI1BDH = 0x02;  // Baud Div = 24MHz/(16x2400) = 625 =0x271
  SCI1BDL = 0x71;    // MSB of baud rate registers
  SCI1CR1 = 0xA0;
  SCI1CR2 = 0x24;    // enable receive and transmit
}

char getcSCI1(){
  while(!(SCI1SR1 & 0x20)){}
  SCI1SR1;
  return (SCI1DRL);
}

#pragma CODE_SEG NON_BANKED

interrupt 21 void SCI_INT(){

  int val;
  int i = 0;
  int bytesRead;
  if((val = getcSCI1()) > 0){
      if(val == 0x0A){
        bytesRead = 0;
        i = 0;
        while(bytesRead < 10){
          if(SCI1DRL > 0){
            val = getcSCI1();
            if((val == 0x0A) || (val == 0x0D)){
              break;
            }
            
            code[bytesRead] = val;
            bytesRead++;
            i++;
          }
          if(bytesRead == 10){
            code[10] = '\0';
          }
        }
      }
    }
    if(i == 10){
      printf("Tag code is: %s\n\r", code);
      i = 0;
    }
}

#pragma CODE_SEG DEFAULT

void delay(int del){
  int i,j;
    for(i=0; i<del; i++)
       for(j=0; j<2000; j++);   
}

2,990 次查看
charlesbrown
Contributor I

I'm trying to use a Parallax RFID for a project and hope that you would be willing to send me your complete code.

0 项奖励
回复

2,990 次查看
eliezeroc
Contributor III

Hello friend, I'm trying to read TAG 1K with EN 60 and RFID-RC522a but I failed. You have any ideas to help me?

Thanks,

0 项奖励
回复

2,990 次查看
hull
Contributor I

Thanks for sharing your code. I'll try it.

0 项奖励
回复