PWM read on HCS12 (Dragon 12)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM read on HCS12 (Dragon 12)

3,775 Views
dragonVStiger
Contributor I

I am having a problem reading a pwm signal into my HCS12. I am using codewarrior. I have been working on this problem for a long time with limited to no success. I am using input capture to time rising and falling edges on the samee channel(0). At this point my interupt is only firing on rising eges, but i think i have the register set correctly for both rising and falling. Any advice would be greatly appreciated.

Here is what i have:

#include <hidef.h>      /* common defines and macros */
#include <mc9s12dg256.h>     /* derivative information */
#pragma LINK_INFO DERIVATIVE "mc9s12dg256b"
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <math.h>
#include "main_asm.h" /* interface to the assembly module */
#define DLC_DELAY 300
#define PI 3.14159265

__interrupt void RealTimeInterrupt( void );
__interrupt void TC0Interrupt( void );
__interrupt void TOI (void);


int diff,rise,fall,last,ovcnt,avg,sum,cnt;
char string[17];
int debug = 55,debug1=60;
int flag = 0;
double dblsum;


void main( void ){
 
  PLL_init();
  LCD_init();
 
 
  DDRT= 0x00;                  //input

  TIOS &= ~0x01;               // channel 0 input capture
                                
  TSCR1= 0x80;                 // enable timer
   
  TIE = 1;                     // timer interupt enable
   
  TSCR2= 0b101;                // prescale 32
   
  TCTL4 = 0b11;                // capture any edge
   
  EnableInterrupts;
 
  
  while(1){   
   

    sum = sum + diff ;
  
 
    if (cnt==100){
   
   
      dblsum=sum ;
      avg = dblsum/cnt;
     

      cnt = 0;
      sum = 0;
    }
 
    }

}

__interrupt void RealTimeInterrupt( void )
{
  CRGFLG = 0x80;       /* clear rti flag */
}

__interrupt void TC0Interrupt( void )
{
  
  TFLG1 = 0x01;     //clear TC0 flag
 
  if(PTT &= 0x01){      //PT0 is high afte interupt   
    rise = TC0;
      
  } else                   //PT0 is low afte interupt
 
  {
  
    fall = TC0;
    diff = fall - rise;
    cnt++ ;
       
  }

}

__interrupt void TOI( void )
{
  
}

 

Labels (1)
0 Kudos
Reply
2 Replies

1,737 Views
dragonVStiger
Contributor I

I have made some progess. My averging was causeing some problems, so i bypassed it. I am getting very accurate readings on the low end of my desired scale (1ms-10ms), but around 10ms and above i am getting an occasional extermly high reading, as the hightime lengthens this error occurs more frequently.  Here's what i have now.

#include <hidef.h>      /* common defines and macros */
#include <mc9s12dg256.h>     /* derivative information */
#pragma LINK_INFO DERIVATIVE "mc9s12dg256b"
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <math.h>
#include "main_asm.h" /* interface to the assembly module */
#define DLC_DELAY 300
#define PI 3.14159265

__interrupt void RealTimeInterrupt( void );
__interrupt void TC0Interrupt( void );
__interrupt void TOI( void );


volatile long unsigned int diff,rise,fall,last,ovcnt,sum=0,cnt,avg;
//float avg;
char string[17];
int debug = 1,debug2=2,debug3=3;
int flag = 0,flag2=0,flag3=0;
double dblsum;


void main( void ){
 
  PLL_init();
  LCD_init();
  DDRT=0x00;                  //input
                              
  TSCR1=  0x80;                 // enable timer
  TSCR2=  0b101;                // prescale 32
  TIOS &= ~0x01;               // channel 0 input capture
  TCTL4 =  0b11;                // capture any edge on channel 0
  TIE =   1;                     // timer interupt enable
   
  EnableInterrupts;
 
  
  while(1){   
   
    if(flag==1){
   
    sprintf(string,"%16d",debug);
    writeLine(string, 1); //write to screen
    flag=0;
   
    }
    if(flag2==1){
   
    sprintf(string,"%16d",debug2);
    writeLine(string, 1); //write to screen
    flag2=0;
   
    }
   
    if(flag3==1){
   
    sprintf(string,"%16d",debug3);
    writeLine(string, 1);         
  
    flag3=0;
   
    }
   
    sum = sum + diff ;
  
 
    if (cnt>10){
     
      //avg = (float) (sum) / (float) (cnt);
      avg = sum/cnt;
      cnt = 0;
      sum = 0;
     
      sprintf(string,"%16lu",diff);
      writeLine(string, 2); //write to screen
      flag2=0;
    }
  }

}

__interrupt void RealTimeInterrupt( void )
{
  CRGFLG = 0x80;       /* clear rti flag */
}

__interrupt void TC0Interrupt( void )
{
  
  TFLG1 = 0x01;     //clear TC0 flag
 
 
 
  if(PTIT & 0x01){
   
    rise = TC0;
    flag = 1;  
  } else
 
  {
  
    fall = TC0;
    diff = fall - rise;
   
    fall=0;
    rise=0;
   
    cnt++ ;
   
    flag = 0;
    flag2 = 1;
  
   
   }

 }
 
 __interrupt void TOI( void )
 {
 
    flag2=0;
    flag3 = 1; 
   
 }
 
 

0 Kudos
Reply

1,737 Views
ipa
Contributor III

Hi,

My opinion: in TC0Interrupt routine, you may use PTIT register to

determine the level of input pin: if (PTIT & 0x01)...

Regards,

ipa

0 Kudos
Reply