PE Micro S12Z "Can't program 8 bytes..."

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PE Micro S12Z "Can't program 8 bytes..."

1,441 次查看
hardydragon
Contributor II

Hello S12Z team,

I am trying to flash and this message comes up..

"Can't program 8 bytes to address 0xff0128 because this range isn't included in the selected modules! "

Flash Operation. ... 
Auto-detection is successful. 
File is of type Motorola S-Record Format. 

Device MC9S12ZVMC128_EEPROM 
Programming ....
Programming warning. Can't program 8 bytes to address 0xff0128 because this range isn't included in the selected modules! 
Programming .......
Programming warning. Can't program 8 bytes to address 0xfffdf8 because this range isn't included in the selected modules! 
Programming ........
Device MC9S12ZVMC128_EEPROM 
Program Command Succeeded 
Flash Operation. done 

What I am doing wrong? What I have to change that this doesn't shows up.

Thank you

0 项奖励
回复
3 回复数

1,317 次查看
hardydragon
Contributor II

Hello,

I only want to program Flash.

I just created a new project in codewarrior and used Flash file to target and there I used my own ".S2" file.

0 项奖励
回复

1,317 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

So you use the S12Z Flash Programmer Task and select Flash device, right?

pastedImage_1.png

Regards,

Daniel

0 项奖励
回复

1,317 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The two addresses are not EEPROM but flash.

What do you want to program? EEPROM or Flash?

How did you configured the Flash Programmer?

Regards,

Daniel

0 项奖励
回复