PC-Lint Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PC-Lint Tool

2,832件の閲覧回数
dorin75
Contributor I
Hi !
 
I'm working with the CW 5.7.0 and my target is a MC9S12XDP512 (starterkit from SofTec). I want to compile/link my project with PC-Lint but I dont't have one. Somebody knows where I could download that PC-Lint from ? 
 
Thank you in advance,
Dorin
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,617件の閲覧回数
J2MEJediMaster
Specialist I
I'm puzzled as to your version of CodeWarrior. The reason I wonder is two fold: first, if you're developing for the HC12SX series (I'm working on with MC9S12XDT512 myself), the latest version of Codewarrior is 4.5. Second, when you use the CW 4.5 Wizard to build the project, it offers to set the the project up for PC-lint. So, you should be able to use PC-lint through using of the setup wizard.

However, I'll have to emphasize that as a moderator, I have the deluxe software installation. :smileyhappy: You'll have to purchase PC-lint from Gimpbel software. If you do, then Codewarrior integrates with it well through its setup wizard.

---Tom

Message Edited by J2MEJediMaster on 2006-09-08 10:01 AM

0 件の賞賛
返信

1,617件の閲覧回数
DanielM
Contributor III
Hi,

as far as I know PC-Lint is a comercial product by Gimpel Software (http://www.gimpel.com/). You will have to buy it from them.

Daniel
0 件の賞賛
返信