P9ZVLA12MLC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,132件の閲覧回数
riccardozamuner
Contributor I

Hello everyone,

 

I'm working on P9ZVLA12MLC0N37P chip, but I'm not able to fine the correct flash size.

If I follow the package information flash should be 12 kbyte but MC9S12ZVL Family Reference Manual

doesn't report that flash size.

 

Any suggestion?

 

Thanks in advanced

ラベル(1)
0 件の賞賛
返信
1 解決策
2,072件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Riccardo,

According our numbering rules, the number of chars in part number is limited.

So, for some part numbers, we have to strip the last significant number from flash size to keep the maximum number characters in part number.

So, the 12 in your part number means 128kB of Flash size.

Similar typical case is S12XEP100 where 100 means 1000kB(1MB) of Flash.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,073件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Riccardo,

According our numbering rules, the number of chars in part number is limited.

So, for some part numbers, we have to strip the last significant number from flash size to keep the maximum number characters in part number.

So, the 12 in your part number means 128kB of Flash size.

Similar typical case is S12XEP100 where 100 means 1000kB(1MB) of Flash.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,072件の閲覧回数
riccardozamuner
Contributor I

Hi RadekS

thank you for your reply.

This solve my problem and explains some test result.

Have a great day too.

Riccardo

0 件の賞賛
返信