P&E BDM Communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P&E BDM Communication

2,257件の閲覧回数
GTM
Contributor I

Hello NXP,

I want to use freemaster by BDM, but the freemaster cannot recognize my multilink fx.

freemaster.png

0 件の賞賛
返信
2 返答(返信)

2,243件の閲覧回数
GTM
Contributor I

I think it is my laptop problem.

usb.png

0 件の賞賛
返信

2,251件の閲覧回数
giraffe508
Contributor IV

Hello,

It seems that FreeMASTER is not recognizing your Multilink FX. To resolve this issue, please follow these steps:

  1. Ensure that you have the latest version of FreeMASTER installed. You can download it from the following link: FreeMASTER Run-Time Debugging Tool.
  2. Make sure that the P&E drivers are installed correctly. You can download the latest P&E drivers from this link: PEmicro Hardware Interface Drivers.
  3. Check if the Multilink FX is connected properly to your target board and the PC.
  4. Verify that the correct communication plugin is selected in FreeMASTER. To do this, go to the 'Project' menu, then select 'Options' and click on the 'Comm' tab. Choose the 'PEMicro BDM' plugin from the drop-down menu.
  5. Ensure that the correct processor is selected in the FreeMASTER project settings. Go to the 'Project' menu, then select 'Options' and click on the 'MCU' tab. Choose the appropriate processor from the list.

If you have followed these steps and the issue persists, please provide more information about your setup, such as the target MCU, the version of FreeMASTER you are using, and any error messages you are encountering.

Best regards.

0 件の賞賛
返信