Our flash cotent is not sufficient, Can the Dflash used as code flash?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Our flash cotent is not sufficient, Can the Dflash used as code flash?

1,969 次查看
hongjianzhang
Contributor III

Our project has some picture, and our customer want us add more, but our flash rom was not sufficient, so I wander is it possible to put some picture or function in the data flash.But when I test putted a const data in the dflash and compile,  the data was not in the target file, when I putted the data in the p-flash , it was correct! Is it the compilled restrict this or dflash can't excute fucntion?

标记 (2)
0 项奖励
回复
1 回复

1,817 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

you have not mentioned the MCU you use.

However, I think

https://community.nxp.com/thread/450421 

answers your issue.

Best regards,

Ladislav