Newbie question about interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Newbie question about interrupts

3,203件の閲覧回数
M3H0
Contributor I
Hi,
 
It´s only 3 weeks since I started to work with a HCS12 family microcontroller (MC9S12C32+chipS12 demoboard) and I´m quite lost. I have been trying to make a program with interrupts, just a very simple one, which just waits for the RTI to be set before toggleing a led with it´s interrupt handler.
 
I have been reading a lot of stuff about that, but I don´t know if I have really understood it. What I have to do is (I´m programming with Imagecraft´s ICC12 compiler):
 
1- Define the interrupt handler in my c code file, like this
              #pragma interrupt_handler timer_handler
                              ...
                 void timer_handler()
                 {
                        ...
                  }
 
2- Modify my vectors.c file like this:
              
                #pragma abs_address:0xffd0

               /* change the above address if your vector starts elsewhere*/
                void (*interrupt_vectors[])(void) =
               {
                /* to cast a constant, say 0xb600, use (void (*)())0xb600*/
                /* 812A4 vectors starts at 0xff80, but most entries are not used if you use Key Wakeup H, change the start address to 0xffCE and add one entry to the beginning */
               DUMMY_ENTRY, /* BDLC */ /* Key Wakeup J */
                DUMMY_ENTRY,
/* ATD */ /* ATD */
                DUMMY_ENTRY,
/* RESERVED */ /* SCI 1 */
                DUMMY_ENTRY,
/* SCI */
                DUMMY_ENTRY,
/* SPI */
                DUMMY_ENTRY,
/* PAIE */
                DUMMY_ENTRY,
/* PAO */
                DUMMY_ENTRY,
/* TOF */
                DUMMY_ENTRY,
/* HC12 TC7 */
                DUMMY_ENTRY,
/* TC6 */
                DUMMY_ENTRY,
/* TC5 */
                DUMMY_ENTRY,
/* TC4 */
                DUMMY_ENTRY,
/* TC3 */
                DUMMY_ENTRY,
/* TC2 */
                DUMMY_ENTRY,
/* TC1 */
                DUMMY_ENTRY,
/* TC0 */
                timer_handler,      
/* RTI */
                DUMMY_ENTRY,
/* IRQ */
                DUMMY_ENTRY,
/* XIRQ */
                DUMMY_ENTRY,
/* SWI */
               DUMMY_ENTRY, /* ILLOP */
                DUMMY_ENTRY, /* COP */
                DUMMY_ENTRY, /* CLM */
                _start /* RESET */
                };
#pragma end_abs_address
Can anyone tell me if I´m right? and what I have to do with the "vectors.c" file? should I include (#include vectors.c) in my c code?
If anyone could tell where I can find some C coded examples it would be great.
 
THX in advance
M3H0
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,016件の閲覧回数
M3H0
Contributor I
Thank you a lot, I will have a look to that thread
 
Oroitz
0 件の賞賛
返信

2,016件の閲覧回数
J2MEJediMaster
Specialist I
This forum thread has a discussion about setting up interrupts. It also references one or two app notes that might provide source code for you to study.

---Tom
0 件の賞賛
返信