Need help about S12 ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help about S12 ADC

1,740 Views
fanziyu
Contributor IV

Hi

Question1:e6181 workaround:  The ADC  should not be disabled before any flow control request (SEQA,TRIG,RSTA)is finished(all flow control bits are cleared).

so 

 ADC0CTL_0_ADC_SR = 1;//execute ADC soft-reset(SR),ADC enters IDLE state
while(ADC0STS_READY == 0){}
ADC0CTL_0 = 0X00;//ADC is disabled 

or

ADC0CTL_0_ADC_SR = 1;
while(ADC0STS_READY == 0){}

ADC0FLWCTL = 0X80;//need? 

while(0 != ADC0FLWCTL ){}//need?

ADC0CTL_0 = 0X00;//ADC is disabled 

Are both the programs correct?

Question2:ATD clock Frequency is 3MHz.10 bit resolution .Then one conversion time ?

if CSL with 17 command entries,then how much time it will cost toally? more details see attachment

thanks!

Tags (1)
0 Kudos
Reply
2 Replies

1,483 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
As the workaround for e6181 states,
“It is recommended to issue a Sequence Abort Request and to poll bit SEQA to be clear before ADC is disabled via bit ADCEN.”

  ADC0FLWCTL_SEQA = 1;     // Issue a Sequence Abort Request
  while(ADC0FLWCTL_SEQA){} // Wait until aborted
  ADC0CTL_0_ADC_EN = 0;        // Disable ADC‍‍‍

The conversion time was discussed in this thread:
S12ZVLA ADC sampling time 

Regards,
Daniel

0 Kudos
Reply

1,483 Views
fanziyu
Contributor IV

thans for your help.Daniel.I wonder if adc is in idle status,i still have to issue a Sequence Abort Request? 

ADC0CTL_0_ADC_SR = 1;//execute ADC soft-reset(SR),ADC enters IDLE state

0 Kudos
Reply