Multiple CAN buses on the same S12 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple CAN buses on the same S12 MCU

1,747 Views
samsam2010
Contributor I

Hi all,

 

May sound an easy question to some of you, but I am just wondering if it is possible to have more than 1 physical CAN bus on the same MCU, let's say the S12XS256. I think there are 5 CAN TX/RX port on the S12XS256, but I just don't know how to control all 5 separated physical CAN buses from the same main program of the single S12XS256 MCU. I tried to search for those info on the web but failed to find anything useful. Thanks!!!:smileywink:

Labels (1)
0 Kudos
Reply
1 Reply

1,254 Views
Lundin
Senior Contributor IV
As long as your MSCAN driver is re-entrant, you can have as many CAN busses as the chip supports.
0 Kudos
Reply