Multilink Connection Problem S12UF32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multilink Connection Problem S12UF32

ソリューションへジャンプ
2,773件の閲覧回数
srgrace09
Contributor I

I have the BDM setup correctly (according to P&E) and the Multilink can't get the frequency of the device. Is anyone else having a problem, or do I need to contact P&E directly?

 

Thanks for any help. 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,022件の閲覧回数
kef
Specialist I

Did you look at UF32 erratas? If not, then read maskset number from your chip case, like 1L47S, and go here

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?ProdMetaId=PID%2FDC%2FS12UF&isAdvanceSearc...&

 

MUCts01498 errata has YES in workaround column, but in fact you can't unsecure secured chip over BDM.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,022件の閲覧回数
srgrace09
Contributor I
I am using Rev.A of the P&E Multilink. I had it working earlier (with an IO_DELAY_CNT of 16). After trying to install a program onto it, I believe the secure bits (bytes) were written, and from what P&E said, this is the only chip that can't be unsecured? I'm in a real bind, and need an answer quickly. Is there a way I can unsecure it?
0 件の賞賛
返信
2,023件の閲覧回数
kef
Specialist I

Did you look at UF32 erratas? If not, then read maskset number from your chip case, like 1L47S, and go here

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?ProdMetaId=PID%2FDC%2FS12UF&isAdvanceSearc...&

 

MUCts01498 errata has YES in workaround column, but in fact you can't unsecure secured chip over BDM.

0 件の賞賛
返信
2,022件の閲覧回数
srgrace09
Contributor I

Thanks for the input! I'll look at it and see what I can do with it. Luckily I have a backup chip for a case like this, so now I know how to get around this silly issue. 

0 件の賞賛
返信