Minimum motor drive supply voltage with GDU Boost

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Minimum motor drive supply voltage with GDU Boost

跳至解决方案
2,110 次查看
pratibhasurabhi
Contributor V

Hello All,

I am using S12 MagniV ZVML64 [GDUV4]. I have the GDU boost option "enabled" and is verified by probing the VSUP and VLS_OUT signal

Given this setting , "theoretically speaking"  what could be the minimum motor driving supply voltage [Vsup] 

标记 (3)
0 项奖励
回复
1 解答
2,086 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @pratibhasurabhi,

The boost converter is operational until the MCU is reset by the Low-voltage reset (LVR) circuit.

AN5207 Hardware Design Guidelines for S12ZVM Microcontrollers

Section 7.7 Boost converter shows a design example with Vin = 3.5V, Vout = 11 and 70mA load.

 

Regards,

Daniel

在原帖中查看解决方案

1 回复
2,087 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @pratibhasurabhi,

The boost converter is operational until the MCU is reset by the Low-voltage reset (LVR) circuit.

AN5207 Hardware Design Guidelines for S12ZVM Microcontrollers

Section 7.7 Boost converter shows a design example with Vin = 3.5V, Vout = 11 and 70mA load.

 

Regards,

Daniel