Memory Errors MC9S12DG256 using CW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory Errors MC9S12DG256 using CW

2,596 Views
PhattieM
Contributor I
As per my previous posts I've been working on my own PCB board to autonomously control a dynamic suspension.  I've finally got the SPI interfaces to work (thanks everyone).  But after some modifications to the board I am recieving error messages that apparently render the board useless (the code doesn't upload).  They are:

FP: FLASH_4000 flash module is bad or protected.
FP: FLASH_C000 flash module is bad or protected.

I've tried unsecuring to no avail.  Any ideas?

TIA,

Mark
Labels (1)
0 Kudos
Reply
1 Reply

1,834 Views
J2MEJediMaster
Specialist I
As the error messages state, you've got a problem when trying to write to Flash memory. If you were writing and storing to Flash memory prior to your modifications, then whatever you changed on the board has affected Flash memory, Check the addressing lines, and whether or not you've got sufficient voltage to program Flash.

---Tom
0 Kudos
Reply