Max voltage can be applied for BLDC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Max voltage can be applied for BLDC

1,359 次查看
miko7895
Contributor I

Hello;

i am using MC9s12ZVMx12EVB and using the example for BLDC motor control with the freeMaster (BLDC sensorless) described in AN4704.

the motor runs with no problem, i need to know the max voltage can be applied on the board as i need to operate BLDC with voltage 48V

if the board can operate do i need to change in the software?

0 项奖励
回复
1 回复

1,255 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

MagniV MCUs target 12V automotive applications.

The the following application notes discuss MagniV in 24V and 48V applications.

AN11967 S12ZVM Family in 48 V Applications 

AN5082 MagniV in 24V Applications

Regards,

Daniel