Max Current From Ballast Transistor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Max Current From Ballast Transistor

1,436 次查看
gordonp
Contributor III

How much current can the external ballast transistor supply when used in conjunction with the 9S12ZVCA processor BCTL pin?

1 回复

1,221 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

This is not defined, only max current IDDX without the external PNP (see Table E-1 of the RM). If the current exceeds this value, the external PNP is required. BCTL provides the base current of the transistor. The Table E-1 provides minimal base current that can be guaranteed. Then the gain of the transistor controls the maximum available current.

 

Please refer to Hardware Design Guidelines for S12ZVC for more information.

 

Regards,

Daniel