Mass erasing paged memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mass erasing paged memory

ソリューションへジャンプ
5,116件の閲覧回数
robynyost
Contributor II

Chip: MC9S12C128

 

I have a program that resides in both paged and unpaged memory.  The program loads fine through the IDE.  However, I am working on a CAN bootloader and being able to program the chip through a GUI using the P&E unit_12z libraries. Right now, I am having problems with erasing the second page of paged memory.

 

I do a mass erase command.  That erases the unpaged memory and the first page of paged memory.  That makes since as that is all that is in flash.  I have tried to set the PPAGE register to 0x39 before a mass erase to erase the second page of paged memory but it doesn't have any effect.  Is there something I am missing?  How do you mass erase the paged memory?

 

The code snipet is:

 

    // Mass erase flash
   write_data_byte(0x100, 0x49);// set FCLKDIV clock divider
   write_data_byte(0x103, 0);   // FCFNG select block 0
   write_data_byte(0x102, 0x10);// set the WRALL bit in FTSTMOD to affect all blocks
   write_data_byte(0x104, 0xFF);// FPROT all protection disabled
   write_data_byte(0x105, 0x30);// clear PVIOL and ACCERR in FSTAT register
   write_data_byte(0x106, 0x41);// write MASS ERASE command in FCMD register
   write_data_byte(0x105, 0x80);// clear CBEIF in FSTAT register to execute the command
   Sleep(2000);                   // wait for command to complete

 

   // Reprogram Security byte to Unsecure state
   write_data_byte(0x100, 0x49);// set FCLKDIV clock divider
   write_data_byte(0x103, 0);   // FCFNG select block 0
   write_data_byte(0x104, 0xFF);

// FPROT all protection disabled

   write_data_byte(0x105, 0x30);// clear PVIOL and ACCERR in FSTAT register
   write_data_word(0xFF0E, 0xFFFE); // write security byte to "Unsecured" state
   write_data_byte(0x106, 0x20);// write MEMORY PROGRAM command in FCMD register
   write_data_byte(0x105, 0x80);// clear CBEIF in FSTAT register to execute the command
   Sleep(2000);                   // wait for command to complete

 

    // Mass erase flash
   write_data_byte(0x100, 0x49);// set FCLKDIV clock divider
   write_data_byte(0x103, 0);   // FCFNG select block 0
   write_data_byte(0x102, 0x10);// set the WRALL bit in FTSTMOD to affect all blocks
   write_data_byte(0x104, 0xFF);// FPROT all protection disabled
   write_data_byte(0x105, 0x30);// clear PVIOL and ACCERR in FSTAT register
write_data_byte(0x30, 0x39);// Set the PPAGE register to the next page
   write_data_byte(0x106, 0x41);// write MASS ERASE command in FCMD register
   write_data_byte(0x105, 0x80);// clear CBEIF in FSTAT register to execute the command
   Sleep(2000);                   // wait for command to complete



   bReturn = set_speed();

 

 


ラベル(1)
1 解決策
4,574件の閲覧回数
robynyost
Contributor II

The code was actually fine.  My error was in reading the values after the mass erase.  Thanks to all!

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,575件の閲覧回数
robynyost
Contributor II

The code was actually fine.  My error was in reading the values after the mass erase.  Thanks to all!

0 件の賞賛
返信
4,574件の閲覧回数
kef
Specialist I

To speedup debugging and memory browsing, Hiwave debugger caches contents of flash memory. To see what really happens after you execute your erase and program routines, you need to go find Memory mapping dialog in Hiwave debugger and set some checkboxes to enable flash memory refreshing when you halt your MCU.

Mass erase, when it succeeds, erases all the flash on S12C. It can't erase just one flash page or some pages, but all the flash. Also, mass erase command won't erase anything in case any part of flash is write protected, and this makes it not useful for application in bootloader. Good bootloader should be never erased from flash memory, because bad things happen and MCU can be unpowered or reset while bootloader is erased, which will brick your product. Instead of mass erase you should erase your application code sector by sector.

You mass erase snipped has a bug. Even for erase command you need to write dummy data to flash array, like you do when programming security byte

write_data_word(0xFF0E, 0xFFFE); // write security byte to "Unsecured" state.

When using secor erase command, writing to particular flash memory sector specifies which sector of flash is going to be erased.

You can't unprotect flash when operating in normal mode, so you need to review this

write_data_byte(0x104, 0xFF); // FPROT all protection disabled

Don't forget that flash memory is not readable while any flash command is in progress, or when you are applying backdoor unsecure key. So you need to move part of your code to RAM and execute from there. Use forums search to find how to do that.

4,574件の閲覧回数
robynyost
Contributor II

Thank you for the help!  My problem is really two fold.  1) Programming everything (including bootloader) through the BDM using a GUI.  2) Writing the CAN bootloader.

This is mainly about #1.  The code was originally this:

// Mass erase flash
   write_data_byte(0x100, 0x49);// set FCLKDIV clock divider
   write_data_byte(0x103, 0);   // FCFNG select block 0
   write_data_byte(0x102, 0x10);// set the WRALL bit in FTSTMOD to affect all blocks
   write_data_byte(0x104, 0xFF);// FPROT all protection disabled
   write_data_byte(0x105, 0x30);// clear PVIOL and ACCERR in FSTAT register
write_data_byte(0x4000, 0xFF);
   write_data_byte(0x106, 0x41);// write MASS ERASE command in FCMD register
   write_data_byte(0x105, 0x80);// clear CBEIF in FSTAT register to execute the command
   Sleep(2000);                   // wait for command to complete

   // Reprogram Security byte to Unsecure state
   write_data_byte(0x100, 0x49);// set FCLKDIV clock divider
   write_data_byte(0x103, 0);   // FCFNG select block 0
   write_data_byte(0x104, 0xFF);

// FPROT all protection disabled

   write_data_byte(0x105, 0x30);// clear PVIOL and ACCERR in FSTAT register
   write_data_word(0xFF0E, 0xFFFE); // write security byte to "Unsecured" state
   write_data_byte(0x106, 0x20);// write MEMORY PROGRAM command in FCMD register
   write_data_byte(0x105, 0x80);// clear CBEIF in FSTAT register to execute the command
   Sleep(2000);                  


The problem is that it is NOT erasing everything.  I read the data bytes after this to verify.  0x400 to 0x7FFF is erased.  0xC000 to 0xFFFF is erased.  0x388000 to 0x38BFFF is erased.  But 0x398000 to 0x39BFFF is NOT erased.  It is erasing most but not all of the memory.


I have tried to do a sector erase too.  That doesn't seem to work either.  Could it be the chip?  Or is there something special to erase the paged memory???


I'm still confused....

0 件の賞賛
返信
4,574件の閲覧回数
kef
Specialist I
  • My problem is really two fold.  1) Programming everything (including bootloader) through the BDM using a GUI.

You are on the wrong track then. For secure application, bootloader should be programmed once and write protected. 

  • // Mass erase flash 
        write_data_byte(0x100, 0x49); // set FCLKDIV clock divider
        write_data_byte(0x103, 0);    // FCFNG select block 0
        write_data_byte(0x102, 0x10); // set the WRALL bit in FTSTMOD to affect all blocks
        write_data_byte(0x104, 0xFF); // FPROT all protection disabled
        write_data_byte(0x105, 0x30); // clear PVIOL and ACCERR in FSTAT register

  • write_data_byte(0x4000, 0xFF);  

^^ this last line is a new bug. You can't write to flash byte or misaligned word.


  •     write_data_byte(0x106, 0x41); // write MASS ERASE command in FCMD register
        write_data_byte(0x105, 0x80); // clear CBEIF in FSTAT register to execute the command
        Sleep(2000);                    // wait for command to complete

Instead of waiting here for fixed? amount of time here, you should wait for CCIF  flag.


  • The problem is that it is NOT erasing everything.  I read the data bytes after this to verify.  0x400 to 0x7FFF is erased.  0xC000 to 0xFFFF is erased.  0x388000 to 0x38BFFF is erased.  But 0x398000 to 0x39BFFF is NOT erased.  It is erasing most but not all of the memory.

Did you check memory mapping in debugger? Isn't debugger fooling you showing you what was there in flash at initial flash programming over BDM? Again, mass erase on S12C128 either fails to erase anything, or erases everything.

  • I have tried to do a sector erase too.  That doesn't seem to work either.

It could be the same effect of debugger not refreshing memory views from device memory.

4,574件の閲覧回数
robynyost
Contributor II

I really do appreciate the help.  I am still having problems.  I have changed what you suggested.  It now reads:

/ Mass erase flash
   write_data_byte(0x100, 0x49);// set FCLKDIV clock divider
   write_data_byte(0x103, 0);   // FCFNG select block 0
   write_data_byte(0x102, 0x10);// set the WRALL bit in FTSTMOD to affect all blocks
   write_data_byte(0x104, 0xFF);// FPROT all protection disabled
   write_data_byte(0x105, 0x30);// clear PVIOL and ACCERR in FSTAT register
write_data_word(0x4000, 0xFFFF);
   write_data_byte(0x106, 0x41);// write MASS ERASE command in FCMD register
   write_data_byte(0x105, 0x80);// clear CBEIF in FSTAT register to execute the command
  

UINT8 cFSTAT = read_data_byte(0x105);

while ((cFSTAT & 0xC0) == 0)

{

    cFSTAT = read_data_byte(0x105);

}

   // Reprogram Security byte to Unsecure state
   write_data_byte(0x100, 0x49);// set FCLKDIV clock divider
   write_data_byte(0x103, 0);   // FCFNG select block 0
   write_data_byte(0x104, 0xFF);

// FPROT all protection disabled

   write_data_byte(0x105, 0x30);// clear PVIOL and ACCERR in FSTAT register
   write_data_word(0xFF0E, 0xFFFE); // write security byte to "Unsecured" state
   write_data_byte(0x106, 0x20);// write MEMORY PROGRAM command in FCMD register
   write_data_byte(0x105, 0x80);// clear CBEIF in FSTAT register to execute the command
  

cFSTAT = read_data_byte(0x105);

while ((cFSTAT & 0xC0) == 0)

{

    cFSTAT = read_data_byte(0x105);

}

I am getting the same results.  I am not going through the HIWAVE program.  I am using the P&E multilink unit12z libraries.  I have no idea what they do under the covers.  After all this is over, I am reading the words out of flash and it is cleared for all memory addresses except for page 0x39.  Any ideas??


0 件の賞賛
返信
4,572件の閲覧回数
RadekS
NXP Employee
NXP Employee

There is procedure from datasheet:

Special single chip erase and unsecure sequence:

1. Reset into special single chip mode.

2. Write an appropriate value to the ECLKDIV register for correct timing.

3. Write 0xFF to the EPROT register to disable protection.

4. Write 0x30 to the ESTAT register to clear the PVIOL and ACCERR bits.

5. Write 0x0000 to the EDATA register (0x011A–0x011B).

6. Write 0x0000 to the EADDR register (0x0118–0x0119).

7. Write 0x41 (mass erase) to the ECMD register.

8. Write 0x80 to the ESTAT register to clear CBEIF.

9. Write an appropriate value to the FCLKDIV register for correct timing.

10. Write 0x00 to the FCNFG register to select Flash block 0.

11. Write 0x10 to the FTSTMOD register (0x0102) to set the WRALL bit, so the following writes

affect all Flash blocks.

12. Write 0xFF to the FPROT register to disable protection.

13. Write 0x30 to the FSTAT register to clear the PVIOL and ACCERR bits.

14. Write 0x0000 to the FDATA register (0x010A–0x010B).

15. Write 0x0000 to the FADDR register (0x0108–0x0109).

16. Write 0x41 (mass erase) to the FCMD register.

17. Write 0x80 to the FSTAT register to clear CBEIF.

18. Wait until all CCIF flags are set.

19. Reset back into special single chip mode.

20. Write an appropriate value to the FCLKDIV register for correct timing.

21. Write 0x00 to the FCNFG register to select Flash block 0.

22. Write 0xFF to the FPROT register to disable protection.

23. Write 0xFFBE to Flash address 0xFF0E.

24. Write 0x20 (program) to the FCMD register.

25. Write 0x80 to the FSTAT register to clear CBEIF.

26. Wait until the CCIF flag in FSTAT is are set.

27. Reset into any mode.

Anyway I would like to recommend “copy” mass erase procedure from PEmicro command file (in attachment).

I think that there could be some issue with FAIL flag in FSTAT register.