Machine exception

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Machine exception

10,813 Views
kaarthichandras
Contributor II

I am using s12zvml31 controller. When i tried to debug my software the machine exception occurs and i saw the datasheets and checked the registers mmcec and mmccc,

Error code register

Bit Field Values:
ITR bits[ 15:12 ] = 1 S12ZCPU
TGT bits[ 11:8 ] = 1
ACC bits[ 7:4 ] = 1 Opcode fetch
ERR bits[ 3:0 ] = 1 Access to an ilegal address range

Captured S12ZCPU Condition Code Register

Bit Field Values:
CPUU bits[ 15:15 ] = 0
bits[ 14:14 ] = 0
bits[ 13:13 ] = 0
bits[ 12:12 ] = 0
bits[ 11:11 ] = 0
bits[ 10:10 ] = 0
bits[ 9:9 ] = 0
bits[ 8:8 ] = 0
bits[ 7:7 ] = 0
CPUX bits[ 6:6 ] = 1
bits[ 5:5 ] = 0
CPUI bits[ 4:4 ] = 1
bits[ 3:3 ] = 0
bits[ 2:2 ] = 0
bits[ 1:1 ] = 0
bits[ 0:0 ] = 0

I have tried the exception handler by writing CPMUARMCOP register to reset the controller and Im not writing any instruction at last 8 bytes of RAM, ROM. Am I missing anything?

Please help me to found out.

Regards

kaarthi

0 Kudos
Reply
20 Replies

10,291 Views
kef2
Senior Contributor V

Hi,

You should start inspecting code at address MMCPC points to. Perhaps some legacy code expects 16 bits code pointers and does some ptr-int-ptr conversions?

Edward

0 Kudos
Reply

10,291 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Edward,

I checked the Kaarthi's code and the machine exception occur after enabling interrupts in the PE init function and Kaarthi recognizes that exception did not occur when the timer interrupt is disabled.

Best regards,

Diana

0 Kudos
Reply

10,291 Views
kef2
Senior Contributor V

Hi Diana,

OK, then either interrupt vector is wrong, or ISR does something wrong. In first case address in MMCPC contains no useful information, in 2nd it may point to address with buggy code.

Edward

0 Kudos
Reply

10,291 Views
kaarthichandras
Contributor II

Thanks Edward and Diana,

The timer interrupt doesn’t have problem, because I have tried several ways to find the problem and with or without timer interrupt I see no difference, the other functions only making a part.

Note: I said that “exception did not occur when the timer interrupt is disabled” only with no other functions because I wanted to check whether the problem is with that interrupt or others.

I hope you understand.

Regards

kaarthi

0 Kudos
Reply

10,291 Views
kaarthichandras
Contributor II

Thanks Edward,

I checked the address that pointed by MMCPC register and that address points to non accessible memory of controller and cross checked the .map file, there is no such address.

Regards

Kaarthi

Sent from my Sony Xperia™ smartphone

-


kef2 wrote -


NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Machine exception

reply from Edward Karpicz<https://community.nxp.com/people/kef2?et=watches.email.thread> in S12 / MagniV Microcontrollers - View the full discussion<https://community.nxp.com/message/1040667?commentID=1040667&et=watches.email.thread#comment-1040667>

0 Kudos
Reply

10,291 Views
kef2
Senior Contributor V

Hi Kaarthi ,

I'll experiment later at free time how S12Z exceptions behave (MMCPC and status bits) on bad interrupt vector perhaps due to accidental overwrite of IVBR, or jump to wrong address or return to wrong address due perhaps stack overflow.

At now we have a lot of unknowns. Could you create copy project to share with sensitive IP removed but problem still shown? I could try figuring what's wrong on S12ZVC, I don't have S12ZVML.

Edward

0 Kudos
Reply

10,287 Views
kef2
Senior Contributor V

Hi,

I tried a bit. On jump from buggy code to not implemented address

ITR bits[ 15:12 ] = 1 S12ZCPU
TGT bits[ 11:8 ] = 0  <---- different to yours
ACC bits[ 7:4 ] = 1 Opcode fetch
ERR bits[ 3:0 ] = 1 Access to an ilegal address range

and MMCPC points exactly to CPU instruction, which performed wrong jump.

On servicing interrupt while interrupt vector points to non implemented address or pointing to registers space (TGT==1), MMCEC is exactly as you wrote, all MMCEC fields  = 1, MMCPC points to unrelated address. Issuing SWI with bad SWI vector MMCPC shows FFFFF0. I didn't check whether it changes servicing different interrupt vectors.

So please double check your interrupt vectors and perhaps IVBR.

Edward

0 Kudos
Reply

10,291 Views
kaarthichandras
Contributor II

Thanks Edward,

I attached a screenshot of register value when I get exception and check the MMCPC register, it is actually a non-accessible memory. 

And I removed all the interrupts from my code.

Capture3.PNGCapture4.PNG

Regards

kaarthi

0 Kudos
Reply

10,291 Views
kef2
Senior Contributor V

Well, some debugging is required, a waste of time without the code, sorry

Edward

0 Kudos
Reply

10,291 Views
kaarthichandras
Contributor II

Thanks Edward,

I have attached the code here(s12_led1), please check it.

And the library file in folder as “STDINC.H”

Regards

kaarthi

0 Kudos
Reply

10,291 Views
kef2
Senior Contributor V

Hi Kaarthi,

Such simple error and such bizarre behavior. Why MMCPC showed weird address about 0x008xxx? Because your code is at about 0xFF8xxx. Why no leading FF in MMCPC? Because not nice coding error made top byte of return address overwritten with 00.

See in events.c

GLOBAL VOID ReadInputs(VOID)

{

BYTE data[1],changed_mask,i;

Size of data array is 1, yet you loop assumes data size 2:

    for (i = 0; i < 2; ++i)... data[i]

Edward

 

0 Kudos
Reply

10,291 Views
kaarthichandras
Contributor II

Thanks Edward,

I corrected that bug but still I’m getting the problem. For testing I even tried without that function, but problem continues.

Regards

kaarthi

0 Kudos
Reply

10,291 Views
kef2
Senior Contributor V

Hi,

then it is another problem. How could I reproduce it?

You code in *.rar worked with periodic interrupt bean disabled. Once enabled it quickly run into exception. Fixing data[1]->data[2] issue solved it completely. Perhaps just on my s12zvc? Not possible to reproduce - not possible to fix.

Edward

0 Kudos
Reply

10,291 Views
kaarthichandras
Contributor II

Thank Edward,

As you said once you enabled the interrupt it ran to exception, is there anything wrong in vector allocation?

Regards

kaarthi

0 Kudos
Reply

10,291 Views
kef2
Senior Contributor V

No. The only problem was BYTE data[1], which had to be fixed to data[2].

Edward

0 Kudos
Reply

10,291 Views
kaarthichandras
Contributor II

Hi Edward,

Thanks for your support.

I finally got the issue solved somewhat.

Now I’m working in ADC part in this controller and I have the doubt in this.

I have wrote those command sequence lists and result sequence lists and configured the GDU peripheral and PTU. When will the ADC interrupt occur? Does it require any trigger from PTU and when will the conversions start?

Regards

kaarthi

0 Kudos
Reply

10,290 Views
kef2
Senior Contributor V

Hi,

ADC command list is where you set after which conversion to trigger interrupt. IIRC you need to bitwise or your command long word with (1L << 24) to trigger interrupt.

Edward

0 Kudos
Reply

10,290 Views
kaarthichandras
Contributor II

Thanks Edward,

The ADC error interrupt has occurred with restart error and I used PTU to give the trigger to ADC and PTU reload error has occurred..

Regards

Kaarthi

Sent from my Sony Xperia™ smartphone

-


kef2 wrote -


NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Machine exception

reply from Edward Karpicz<https://community.nxp.com/people/kef2?et=watches.email.thread> in S12 / MagniV Microcontrollers - View the full discussion<https://community.nxp.com/message/1045390?commentID=1045390&et=watches.email.thread#comment-1045390>

0 Kudos
Reply

10,290 Views
kaarthichandras
Contributor II

Hi Edward,

I wanted to add ADC1  AN1_3.

 

And then, I modified a code

volatile char ADC0CommandList[6][4]  @0x00001000 = {

{0x40,0xD0,0x00,0x00},

{0xC0,0xCB,0x00,0x00},

{0x00,0x00,0x00,0x00},

{0x00,0x00,0x00,0x00},

{0x00,0x00,0x00,0x00},

{0x00,0x00,0x00,0x00}

};

volatile char ADC1CommandList[6][4]  @0x00001018=

{

{0x40,0xCA,0x00,0x00},

{0xC0,0xD3,0x00,0x00},

{0x00,0x00,0x00,0x00},

{0x00,0x00,0x00,0x00},

{0x00,0x00,0x00,0x00},

{0x00,0x00,0x00,0x00}

};

volatile short PTUTriggerEventList[2][2][3] @0x00001048 =

{

{{0x0100,0x0200,0x0000},{0x0000,0x0000,0x0000}},

{{0x0100,0x0200,0x0000},{0x0000,0x0000,0x0000}}

};

Now Im getting ADC0 and ADC1 trigger error.

How to set the correct configuration?..

Regards

kaarthi

0 Kudos
Reply

10,291 Views
kaarthichandras
Contributor II

I tried again the problem continues here but when I removed DisplOut function it works fine now.

kaarthi

0 Kudos
Reply